Triggerless Mode (Channel Quality)

Triggerless Mode stabilizes the phase between the balanced and unbalanced ch freq response. Triggerless Mode is especially useful when a device under test cannot provide a Trigger Out signal. Triggerless Mode is available when Compute Unbalanced Response is selected.

Enabled - (Default) No trigger is required. 

The stimulus waveform will be doubled in length when this parameter is enabled.

Disabled - A waveform trigger is required to trigger the acquisition at the start of the stimulus waveform.

Triggerless Mode affects the stimulus waveform, so you will need to re-export the stimulus to your signal generator after changing this setting.

See Also

   Analysis Tab (Channel Quality)